990-91138A-001

Specifications for Maintenance Bypass Cabinet with Input Transformer (GVSBPIT25, GVSBPIT50, GVSBPIT75)

UPS rating 10 kW 15 kW 20 kW 25 kW 30 kW 40 kW 50 kW 60 kW 75 kW
Input voltage (V) 480/600
Input connections 3-wire (L1, L2, L3, PE)
Nominal input current (A) 13/10 19/15 26/20 32/26 38/31 51/41 64/51 82/67 100/81
Maximum input current (A) 15/12 23/16 31/25 38/31 46/37 61/49 77/61 95/75 115/92
Output connections 4-wire (L1, L2, L3, N, PE)
Output voltage (V) 208
Nominal output current (A) 28 42 56 69 83 111 139 167 208
Frequency (Hz) 60
Circuit breaker interrupting ratings (kA) 100 at 240 V (for UIB/MBB/UOB)
Continuous operation limited to maximum 110% load.

Trip Settings for Maintenance Bypass Cabinet with Input Transformer

NOTE: Ir, tr, and li must be set during installation. Set the breaker settings per system kW rating as listed in the table below. Changing the settings to other than the listed settings will change the 125% and 150% overload operation, and will impact system performance.
UPS rating Breaker type Ir setting Tr at 6 Ir setting Ir setting Tr at 6 Ir setting li (x In) setting
UIB/MBB/UOB UIB MBB/UOB UIB/MBB/UOB
10 kW HJF36150CU31X 50 0.5 50 0.5 1.5
15 kW HJF36150CU31X 60 0.5 50 4 1.5
20 kW HJF36150CU31X 80 0.5 70 4 1.5
25 kW HJF36150CU31X 100 0.5 80 4 1.5
30 kW JJF36250CU31X 110 4 100 4 1.5
40 kW JJF36250CU31X 150 4 150 4 1.5
50 kW JJF36250CU31X 200 0.5 175 2 1.5
60 kW JJF36250CU31X 250 4 225 1 2
75 kW JJF36250CU31X 250 4 250 2 2

Recommended Upstream Protection for Maintenance Bypass Cabinet with Input Transformer

For 480 V Input

UPS rating Breaker type Ir setting Tr at 6 Ir setting li (x In) setting
10 kW HJL36060U31X 15 4 6
15 kW HJL36060U31X 25 4 6
20 kW HJL36060U31X 30 4 6
25 kW HJL36060U31X 35 4 6
30 kW HJL36060U31X 45 4 12
40 kW HJL36060U31X 60 4 12
50 kW HJL36100U31X 70 4 8
60 kW JJL36250CU31X 100 0.5 2
75 kW JJL36250CU31X 100 0.5 2

For 600 V Input

UPS rating Breaker type Ir setting Tr at 6 Ir setting li (x In) setting
10 kW HJL36060U31X 15 1 6
15 kW HJL36060U31X 20 4 6
20 kW HJL36060U31X 25 4 6
25 kW HJL36060U31X 30 4 6
30 kW HJL36060U31X 35 8 12
40 kW HJL36060U31X 45 8 12
50 kW HJL36060U31X 60 4 12
60 kW JJL36250CU31X 100 0.5 2
75 kW JJL36250CU31X 100 0.5 2

Recommended Cable Sizes for Maintenance Bypass Cabinet with Input Transformer

DANGER
hazard of electric shock, explosion, or arc flash
All wiring must comply with all applicable national and/or electrical codes. The maximum allowable cable size is 4/0 AWG.
Failure to follow these instructions will result in death or serious injury.
NOTE: Overcurrent protection and cable lugs are to be provided by others.

Cable sizes in this manual are based on Table 310.15 (B)(16) of the National Electrical Code (NEC) with the following assertions:

  • 90 °C (194 °F) conductors (75 °C (167 °F) termination)

  • An ambient temperature of 30 °C (86 °F)

  • Use of copper or aluminum conductors

If the ambient temperature is greater than 30 °C (86 °F), larger conductors are to be selected in accordance with the correction factors of the NEC.

Equipment grounding conductors/Protective Earth (PE in this manual) are sized in accordance with NEC Article 250.122 and Table 250.122.

Copper

UPS rating 10 kW 15 kW 20 kW 25 kW 30 kW 40 kW 50 kW 60 kW 75 kW
Input phases (AWG/kcmil) 8 8 8 8 4 4 4 3 1
Input PE (AWG/kcmil) 10 10 10 10 10 8 8 6 6
Output phases (AWG/kcmil) 8 8 4 4 3 1 2/0 3/0 4/0
Output PE (AWG/kcmil) 10 10 8 8 8 6 6 4 4
Neutral (AWG/kcmil)* 8 4 2 1 1/0 3/0 2 x 1 2 x 1/0 2 x 3/0
DC+/DC- (AWG/kcmil) 10 6 4 4 2 1/0 1/0 4/0 2 x 1
DC PE (AWG/kcmil) 10 10 8 8 6 6 6 4 4

Aluminum

UPS rating 10 kW 15 kW 20 kW 25 kW 30 kW 40 kW 50 kW 60 kW 75 kW
Input phases (AWG/kcmil) 6 6 6 6 2 2 2 1  
Input PE (AWG/kcmil) 8 8 8 8 8 6 6 4
Output phases (AWG/kcmil) 6 6 3 2 1 3/0 4/0 2 x 1
Output PE (AWG/kcmil) 8 8 6 6 6 4 4 2
Neutral (AWG/kcmil)* 6 3 1 2/0 3/0 2 x 1 2 x 2/0 2 x 3/0
DC+/DC- (AWG/kcmil) 8 4 3 2 1/0 2/0 2/0  
DC PE (AWG/kcmil) 8 8 6 6 4 4 4
NOTE: DC cables are only connected in the maintenance bypass cabinet in top cable entry systems. In bottom cable entry systems, the DC cables are connected directly in the UPS.
NOTE: The DC cable sizes given here are recommendations – Always follow the specific instructions in the battery solution documentation for DC cable sizes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.