990-5910G-001

Change the Password

NOTE: Always change your password on your first login and keep the password in a secure location.
TIP: Create complex passwords to protect your UPS:
  • The password should be at least eight characters long.

  • The password should be significantly different from previous passwords and from passwords to other devices.

  • Use a combination of uppercase letters, lowercase letters, numbers and special characters.

  1. Tap Logout.
  2. Tap Configuration.
  3. Enter your password.
    NOTE: The default administrator username and password is admin.
  4. Tap Change password and enter the new password.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.