990-5910G-001

Tests

The UPS system can perform the following tests to ensure correct performance of the system:

  • Buzzer

  • Status LEDs

  • Breaker lamp

  • Runtime calibration

  • Battery

Tap the menu button on the home screen and select Maintenance and Buzzer, or Status LEDs, or Breaker lamp to start the test of these functions. See Start a Runtime Calibration Test and Start a Battery Test for details and requirements for these tests.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.