990-5910F-001

Configure High Efficiency Mode

  1. Tap Configuration > High efficiency .
  2. Select the High efficiency mode: Disable, ECO mode, or eConversion.
    NOTE: Contact Schneider Electric to enable ECO mode.
  3. Select eConversion harmonics compensator, if relevant.
  4. Select the High efficiency schedule: Active on schedule, Always active, or Never active.
    1. For Active on schedule, tap Schedule and set up and enable the schedule(s) as needed.
QR code for this page

Was this helpful?