Start a Battery Test
Prerequisites:
-
The battery breakers are closed.
-
No critical alarms present.
-
The bypass supply must be available.
-
Static bypass operation must be available.
-
The batteries must be more than 50% charged.
-
The runtime available must be more than 4 minutes.
-
The operation mode must be normal operation, ECOnversion, or ECO mode.
-
The system operation mode must be inverter, ECOnversion, or ECO mode.
This feature performs a number of tests on the batteries, such as fuse-blown check and weak battery detection. The test will discharge the batteries and use about 10% of the total runtime capacity. Example: If you have 10 minutes of runtime, the test will run for 1 minute. The battery test can be scheduled to run automatically in different time intervals (from weekly and up to once a year).
- Select .
- Tap OK on the confirmation screen.