990-5910G-001

Configure the Disconnect Devices

NOTE: This configuration is mandatory for correct UPS operation.
  1. Tap Configuration > Breakers.
  2. Tap the different disconnect devices in the mimic diagram to configure which disconnect devices are present in the UPS system. Square with a means that the disconnect device is present, empty square means that the disconnect device is not present, grayed out square means that the disconnect device is automatically configured in your UPS system.
    NOTE: The UPS can monitor up to two battery disconnect devices in a standard battery solution. The UPS can monitor up to four battery disconnect devices in a modular battery solution – this is configured automatically by the UPS. The mimic diagram only shows one battery disconnect device BB even if more battery disconnect devices have been connected and configured for monitoring. If one or more of the monitored battery disconnect devices are in the closed position, the BB on the mimic diagram will show as closed. If all of the monitored battery disconnect devices are in the open position, the BB on the mimic diagram will show as open.
  3. Tap OK to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?