990-91582A-001

Connect the Signal Cables in a Dual Mains System

NOTE: Use the signal cables provided in the Galaxy VS cable kit single mains UIB GVSOPT041 and the Galaxy VS cable kit dual mains SSIB GVSOPT042.
NOTE: Connections to 640-4864 are considered Class 2/SELV. Connections to 640-4843 are considered non-Class 2/non-SELV.
  1. Connect the signal cable 0W13750 (breaker indicator lights), the signal cables 0W76723 and 0W13752 (transformer thermal sensor), the signal cables 0W13761 (breaker AUX switches and surge protection device (SPD) alarm signal), and the signal cable 0W13753 (breaker AUX switches and surge protection device (SPD) alarm signal) to the UPS as shown.
    NOTE: The 0W13761 and 0W13753 connection to J6616 pin 5 and 6 is for surge protection device (SPD) alarm signal. Configure input contact 5 and 6 with the function User-defined 1 or User-defined 2 when setting up the input contacts on the UPS display. If other inputs are needed for input contact 5 and 6, the surge protection device (SPD) alarm signal can be removed from J6616 pin 5 and 6.
  2. Route the signal cables down through the cable channel in the left side of the UPS and into input transformer cabinet 1 through the cable entry opening.
    NOTE: Route the signal cables as far away from the power cables as possible to avoid EMC disturbance.
  3. Reconnect the signal cables for input transformer cabinet 1 at the cable connection point in input transformer cabinet 1.
  4. Route the signal cables for input transformer cabinet 2 into input transformer cabinet 2 through the cable entry opening.
  5. Reconnect the signal cables at the cable connection point in input transformer cabinet 2.
  6. Install the SSIB breaker indicator light in input transformer cabinet 2 (the parts are provided in the Galaxy VS cable kit dual mains SSIB GVSOPT042):
    1. Install the SSIB breaker indicator light in the bracket next to the breaker in input transformer cabinet 2.
    2. Connect the signal cable 0W13751 (HSSIB+ and HSSIB-) to the SSIB breaker indicator light (+ and -).
    3. Connect the signal cable 0W13751 from the SSIB breaker indicator light to signal cable 0W13750 at the cable connection point in input transformer cabinet 2.

    Input Transformer Cabinet 2

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?