990-91582A-001

Install the Seismic Anchoring (Option)

Use the optional installation kits GVSOPT002 (for the UPS) and GVSOPT008 (for the input transformer cabinet) for this procedure.
  1. Interconnect the rear anchors for the input transformer cabinet(s) and the UPS with the interconnection plate(s) and four M8 bolts (provided).
  2. Mount the rear anchor assembly to the floor. Use appropriate hardware for the floor type – the hole diameter in the rear anchor is ø14 mm.

    Single Mains System

    Dual Mains System

  3. Install the rear anchoring brackets on the UPS and the input transformer cabinet(s) with the M8 bolts (provided).

    Rear View of the Input Transformer Cabinet

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?