990-91582A-001

Final Installation

  1. Reinstall the transparent plates and the front plates on the input transformer cabinet.

    Front View of the Input Transformer Cabinet

  2. Only for dual mains system: On input transformer cabinet 2, replace the UIB label with the SSIB label, add the indicator light label HSSIB, and replace the diagram label 885-92825 with the diagram label 883-92863. The labels are provided with the Galaxy VS cable kit dual mains SSIB GVSOPT042.

    Single Mains System

    Dual Mains System

  3. Only for seismic anchoring:
    1. Install the seismic front anchoring bracket on the input transformer cabinet(s) with the provided M8 bolts.
    2. Mount the seismic front anchoring bracket on the input transformer cabinet(s) to the floor. Use appropriate hardware for the floor type – the hole diameter in the front anchoring bracket is ø18 mm.

    Front View of the Input Transformer Cabinet

  4. Reinstall the front panel on the input transformer cabinet:
    1. Insert the two tabs in the bottom of the front panel in the input transformer cabinet at a tilted angle.
    2. Reconnect the front panel strap to the input transformer cabinet.
    3. Close the front panel and lock with the two locking knobs.

      Front Right View of the Input Transformer Cabinet

  5. Follow the UPS installation manual to connect the power cables from the input transformer cabinet in the UPS and to complete the rest of the UPS installation.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?