990-91582A-001

Installation Procedure for Dual Mains System

NOTE: The Galaxy VS cable kit single mains UIB GVSOPT041 and the Galaxy VS cable kit dual mains SSIB GVSOPT042 are required for a dual mains system.

Top Cable Entry System

Bottom Cable Entry System

  1. Prepare the Input Transformer Cabinet(s) for Cables.
  2. Install the Seismic Anchoring (Option).
  3. Interconnect the UPS and the Input Transformer Cabinet in a Dual Mains System.
  4. Install the Surge Protection Device (SSP08EMA12).
  5. Follow the installation manual provided with the surge protection device (SSP08EMA12) to connect the power cables and signal cables to the surge protection device.
  6. Connect the Power Cables in the Input Transformer Cabinets in a Duals Mains System.
  7. Connect the Signal Cables in a Dual Mains System.
  8. Final Installation.
  9. Follow the UPS installation manual to connect the power cables from the input transformer cabinet in the UPS and to complete the rest of the UPS installation.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?