Install the Surge Protection Device (SSP08EMA12)
Mounting bracket, washers, and screws are provided in the Galaxy VS cable kit single mains UIB GVSOPT041 and the Galaxy VS cable kit dual mains SSIB GVSOPT042.
- Remove the five preinstalled M6 screws from the top of the input transformer cabinet. Install the mounting bracket on the top of the input transformer cabinet(s) with the five M6 screws.
- Install the surge protection device (SSP08EMA12) on the preinstalled screws and washers on the mounting bracket.
- Remove the top gland plates and the top brush plates from the input transformer cabinet(s).
-
Perform one of the following:
- For installation without conduits: Reinstall the brush plates.
- For installation with conduits: Drill a hole in the gland plates for conduits, install conduits (not provided), and reinstall the gland plates.
- Route the preinstalled power cable from inside the input transformer cabinet(s) out through the left brush plate/gland plate. Follow the installation manual provided with the surge protection device to connect the power cables.
- Route the preinstalled signal cable from inside the input transformer cabinet out through the right brush plate/gland plate. Follow the installation manual provided with the surge protection device to connect the signal cable.