990-91582A-001

Interconnect the UPS and the Input Transformer Cabinet in a Dual Mains System

  1. Remove the three M6 x 16 mm interconnection screws from the right side of the input transformer cabinets. Save for interconnection.

    Front View of the Input Transformer Cabinet

  2. Remove the rear bracket from input transformer cabinet 1.

    Rear View of Input Transformer Cabinet 1

  3. Position input transformer cabinet 2 and input transformer cabinet 1 next to each other.
  4. Install the provided interconnection rear bracket (870-67507) (provided in the Galaxy VS cable kit dual mains SSIB GVSOPT042) between the input transformer cabinets.

    Rear View of Input Transformer Cabinet 2 and Input Transformer Cabinet 1

  5. Install the three M6 x 16 mm interconnection screws between the input transformer cabinets as shown.

    Front View of Input Transformer Cabinet 1 and Input Transformer Cabinet 2

  6. Push the interconnected input transformer cabinets into final position. For seismic anchoring: Align so the rear anchoring bracket on the input transformer cabinets connects to the rear anchors.

    Rear View of Input Transformer Cabinet 2 and Input Transformer Cabinet 1 with Seismic Anchoring

  7. Push the UPS into final position next to input transformer cabinet 2. The rear bracket on input transformer cabinet 2 must connect to the UPS. Align with the rear anchors if seismic anchoring is present.

    Rear View of the UPS and Input Transformer Cabinet 2 and Input Transformer Cabinet 1

  8. Install the three M6 x 16 mm interconnection screws between input transformer cabinet 2 and the UPS as shown.

    Front View of Input Transformer Cabinet 1 and Input Transformer Cabinet 2 and the UPS

  9. Lower the front and rear leveling feet on the UPS and the input transformer cabinets with a wrench until they connect with the floor. Use a bubble-leveler to check that the UPS and input transformer cabinets are level.

    Front View of the UPS

    CAUTION
    Tip hazard
    Do not move the cabinet after the leveling feet have been lowered.
    Failure to follow these instructions can result in injury or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?