990-91582A-001

Connect the Power Cables in the Input Transformer Cabinets in a Duals Mains System

NOTE: Route the input cables, bypass cables, load cables, and DC cables separately to avoid EMC disturbance.
NOTE: Route the power cables in front of the horizontal bracket in the top or bottom of the input transformer cabinet to ensure correct separation from the transformer.
  1. Route the equipment grounding conductor through the top or bottom of input transformer cabinet 1 and input transformer cabinet 2. Connect the equipment grounding conductor to the ground busbar in input transformer cabinet 1 and input transformer cabinet 2.
  2. Route the input cables through the top or bottom of input transformer cabinet 1 and connect the input cables (L1, L2, L3, N) to the 600 V input busbars in input transformer cabinet 1.
  3. Connect the provided UPS input cables (L1, L2, L3, N) to the UPS input busbars in input transformer cabinet 1.

    Front View of Input Transformer Cabinet 1 and Input Transformer Cabinet 2 and the UPS – Top Cable Entry

    Front View of Input Transformer Cabinet 1 and Input Transformer Cabinet 2 and the UPS – Bottom Cable Entry

  4. Route the UPS input cables through the cable entry opening in the left side of input transformer cabinet 1, through input transformer cabinet 2, and into the UPS.
  5. Route the bypass cables through the top or bottom of input transformer cabinet 2 and connect the bypass cables (L1, L2, L3, N) to the 600 V bypass busbars in input transformer cabinet 2.
  6. Connect the provided UPS bypass cables (L1, L2, L3, N) to the UPS bypass busbars in input transformer cabinet 2.
  7. Route the UPS bypass cables through the cable entry opening in the left side of input transformer cabinet 2 and into the UPS.
  8. Perform one of the following:
    • For top cable entry: Route the output cables and the DC cables through the top of input transformer cabinet 2 and through the cable entry opening in the left side of input transformer cabinet 2 and into the UPS.
    • For bottom cable entry: Route the output cables and the DC cables through the bottom of the UPS.
  9. Fasten the power cables to the horizontal bracket in the top or bottom of input transformer cabinet 1 and input transformer cabinet 2 with cable ties.
  10. Follow the UPS installation manual to connect the UPS input cables, the UPS bypass cables, the DC cables, and the output cables in the UPS.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?