Prepare the Input Transformer Cabinet(s) for Cables
DANGER |
|---|
|
Hazard of electric shock, explosion, or arc flash
Do not drill or cut holes for power cables or conduits with the gland plate installed
and do not drill or cut holes in close proximity to the input transformer cabinet.
Failure to follow these instructions will result in death or serious injury.
|
- Remove the front panel and the front plates from the input transformer cabinet(s).
- Remove the transparent plates from the input transformer cabinet(s).
- Remove the left side panel from the UPS and reinstall the side panel on the left side of input transformer cabinet 1.
-
For top cable entry:
- Remove the top cover from the input transformer cabinet(s).
- Remove the gland plate from the top cover.
- Drill or punch holes for power cables or conduits in the gland plate. Conduits are not provided.
- Reinstall the gland plate in the top cover.
- Reinstall the top cover on the input transformer cabinet(s) with four screws.
-
For bottom cable entry:
- Remove the gland plate from the bottom of the input transformer cabinet(s).
- Drill or punch holes for power cables or conduits in the gland plate. Conduits are not provided.
- Reinstall the gland plate in the bottom of the input transformer cabinet(s).
DANGER