990-91582A-001

Interconnect the UPS and the Input Transformer Cabinet in a Single Mains System

  1. Remove the three M6 x 16 mm interconnection screws from the right side of the input transformer cabinet. Save for interconnection.

    Front View of the Input Transformer Cabinet

  2. Push the input transformer cabinet into final position. For seismic anchoring: Align so the rear anchoring bracket on the input transformer cabinet connects to the rear anchor.

    Rear View of the Input Transformer Cabinet with Seismic Anchoring

  3. Push the UPS into final position next to the input transformer cabinet. The rear bracket on the input transformer cabinet must connect to the UPS. Align with the rear anchors if seismic anchoring is present.

    Rear View of the UPS and the Input Transformer Cabinet

  4. Install the three M6 x 16 mm interconnection screws between the input transformer cabinet and the UPS as shown.

    Front View of the Input Transformer Cabinet and the UPS

  5. Lower the front and rear leveling feet on the UPS and the input transformer cabinet with a wrench until they connect with the floor. Use a bubble-leveler to check that the UPS and input transformer cabinet are level.

    Front View of the UPS

    CAUTION
    Tip hazard
    Do not move the cabinet after the leveling feet have been lowered.
    Failure to follow these instructions can result in injury or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?