990-5451L-001

Input Power Factor

  500 kW 625 kW 750 kW 800 kW 1000 kW 1100 kW 1250 kW 1500 kW
25% load 0.98 0.98 0.98 0.98 0.98 0.98 0.98 0.98
50% load 0.99 0.99 0.99 0.99 0.99 0.99 0.99 0.99
75% load 0.99 0.99 0.99 0.99 0.99 0.99 0.99 0.99
100% load 0.99 0.99 0.99 0.99 0.99 0.99 0.99 0.99
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.