990-55111E-001

Connect the Modbus Cables

  1. Connect the Modbus cables to the UPS(s). Use either 2-wire or 4-wire connection.

    Front View

    • All Modbus signal cables shall be double insulated/jacket cable and minimum rated for 30 VDC.

    • Shielded twisted pair cables must be used for Modbus connections. The shield connection to the ground must be as short as possible (ideally below 1 cm). The cable shield must be connected to the Ch Gnd pin on each device.

    • Wiring should be done in accordance with local wiring codes.

    • Route signal cables separately from power cables to ensure sufficient isolation.

    • The Modbus port is galvanically isolated with the Com pin as ground reference.

    Example: 2-Wire Connection with Two UPSs

    Example: 4-Wire Connection with Two UPSs

  2. Install 150 Ohm termination resistors at each end of each bus if the buses are very long and operate at high data rates. Busses under 610 meters at 9600 baud or under 305 meters at 19200 baud should not require termination resistors.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?