990-55111E-001

Decommission or Move the UPS to a New Location

  1. Shut down the UPS completely – follow the instructions in the UPS operation manual.
  2. Lockout/Tagout all disconnect devices in the switchgear in the OFF (open) position.
  3. Lockout/Tagout all battery disconnect devices in the switchgear/battery solution in the OFF (open) position.
  4. Open the front doors of the UPS.
  5. Remove all the power modules from the UPS.
    WARNING
    Heavy load
    Power modules are heavy (54 kg). Use appropriate lifting equipment and trained personnel to lift and handle the power module. It is recommended to use a scissor lifting cart or similar appropriate lifting equipment as shown in this procedure, see Specifications for Recommended Scissor Lifting Cart for details. If no lifting equipment is available, three persons are required to lift and handle the power module.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
    WARNING
    Hazard of injury
    Never stack the power modules on top of each other.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
    CAUTION
    Heavy load and potentially hot surface
    Use protective gloves and safety shoes when handling the power modules.
    Failure to follow these instructions can result in injury or equipment damage.
    1. Set the enable switch to the OFF (unlocked) position. Remove the four screws from the power module.

      Front View

    2. Use the provided power module tool to pull the power module out from the power module slot. Place the tool as shown.

      Front View of Using the Power Module Tool When the Power Module is Next to a Filler Plate

      Front View of Using the Power Module Tool When the Power Module is Next to an Empty Slot

      Front View of Using the Power Module Tool When the Power Module is Next to a Power Module

    3. Pull the power module halfway out. A locking mechanism prevents the power module from being pulled all the way out.
    4. Release the lock by pressing the release button in the right side of the power module and pull the power module out onto an appropriate scissor lifting cart.

      Front View

    5. Install a filler plate in front of the empty power module slot, if available.

      Front View

    WARNING
    risk of equipment damage
    • Store the power modules at an ambient temperature of -25 to 55 °C, 0-95% non-condensing humidity.
    • Store the power modules in their original protective packaging.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  6. Remove the plate from the measurement points. Save for reinstallation.

    Front View

  7. Measure for and verify ABSENCE of voltage with a multimeter probe through the holes in the transparent plate for input, bypass, output, neutral, and DC.

    Front View

  8. Reinstall the plate over the measurement points.
  9. Remove the two inner doors. Save all parts for reinstallation:
    1. Remove the two screws and the two L-shaped parts. Remove the 13 screws.

      Front View

    2. Open the two inner doors.
    3. Unplug the signal cable connectors.
    4. Remove the nut and brackets in both sides.

      Front View

    5. Lift the inner doors upwards to remove them.

      Front View

  10. Measure for and verify ABSENCE of voltage on each input/bypass/output/neutral/DC busbar before continuing.
    DANGER
    hAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Measure for and verify ABSENCE of voltage on each input/bypass/output/neutral/DC busbar before continuing.
    Failure to follow these instructions will result in death or serious injury.

    Front View

  11. Disconnect all power cables from the UPS. See Connect the Power Cables in the UPS for details.
  12. If external sync is present: Remove the transparent protection cover from the external synchronization board 0P4809. Disconnect the signal cables from the external synchronization board 0P4809. See Connect the Signal Cables for External Synchronization for details.
    DANGER
    Hazard of electric shock, explosion, or arc flash
    Check for absence of voltage for all three signal terminals on the external synchronization board 0P4809. When the external synchronization cables are installed, the terminals on the external synchronization board 0P4809 may be energized. Disconnect the fuse disconnector device at the source before removing the transparent protection cover.
    Failure to follow these instructions will result in death or serious injury.

    Front View

  13. Reinstall the two inner doors:
    1. Lift the inner doors onto the hinges.
    2. Reinstall the nut and brackets in both sides.
    3. Reconnect the signal cable connectors.
    4. Close the inner doors and reinstall the 13 screws.
    5. Reinstall the L-shaped part in both sides with the two screws.

    Front View

  14. Disconnect and remove all signal cables from the UPS. See Connect the Signal Cables, Connect the Signal Cables from Switchgear and Third-Party Auxiliary Products, Connect the Modbus Cables, and Connect the PBUS Cables for details.
  15. Only for UPS with seismic anchoring: Remove the front seismic anchoring bracket. Save for reinstallation.
  16. Only for UPS with seismic anchoring: Disconnect the UPS from the rear seismic anchoring bracket by loosening the bolts.

    Front View

  17. Close and lock the front doors.
  18. Raise the feet of the UPS until the casters have full contact with the floor.
  19. You can now move the UPS by rolling it over the floor on the casters.
    WARNING
    TIPPING hazard
    • The casters of the UPS are exclusively for transport on flat, even, hard, and horizontal surfaces.
    • The casters of the UPS are intended for transport over short distances (i.e. inside the same building).
    • Move at a slow pace and pay close attention to the floor conditions and the balance of the UPS.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  20. Only for UPS with seismic anchoring: Remove the rear seismic anchoring bracket from the floor. Save for reinstallation. See Mount the Seismic Anchoring and Position the UPS for details.
  21. For transport over longer distances or in conditions that are not suitable for the casters of the UPS:
    WARNING
    Top-heavy cabinet
    The UPS can be top-heavy with no power modules installed. Take appropriate precautions during handling and preparation for transport/shipment.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
    WARNING
    TIPPING hazard
    For transport over longer distances or in conditions that are not suitable for the casters of the UPS, ensure:
    • that personnel performing the transport have necessary skill and have received adequate training;
    • to use appropriate tools to safely lift and transport the UPS;
    • to protect the product against damage by using appropriate protection (like wrapping or packaging).
    Failure to follow these instructions can result in death, serious injury, or equipment damage.

    Transportation requirements:

    • Mount the UPS in a vertical position in the center of a suitable pallet that can support the weight of the UPS (639 kg with no power modules installed).

    • Use appropriate means of fixation to mount the UPS to the pallet.

    • The original shipping pallet in combination with the original transportation brackets can be reused, if in undamaged condition.

    DANGER
    TIPPING hazard
    • The UPS must be appropriately fixed to the pallet immediately after being placed on the pallet.
    • The fixation hardware must be strong enough to withstand vibrations and shocks during loading, transport, and unloading.
    Failure to follow these instructions will result in death or serious injury.
    WARNING
    Unexpected equipment behavior
    Do not lift the UPS with a forklift/pallet truck directly on the frame as it may bend or damage the frame.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  22. Perform one of the following:
    • Decommission the UPS, OR
    • Move the UPS to a new location to install it.
  23. Only for installing the UPS in a new location: Follow the installation manual to install the UPS in the new location. See Installation Procedure for the UPS for installation overview. Start-up must only be performed by Schneider Electric.
    DANGER
    hAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Start-up must only be performed by Schneider Electric.
    Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?