990-55111E-001

Install the Power Module(s)

The UPS can arrive with or without preinstalled power modules. Additional power modules are shipped separately and must be installed to reach the correct UPS kW rating.
WARNING
Heavy load
Power modules are heavy (54 kg). Use appropriate lifting equipment and trained personnel to lift and handle the power module. It is recommended to use a scissor lifting cart or similar appropriate lifting equipment as shown in this procedure. If no lifting equipment is available, three persons are required to lift and handle the power module.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Specifications for Recommended Scissor Lifting Cart

Lifting weight capacity: Minimum 80 kg
Lifting height range (lowest power module position to highest power module position): 100 mm to 650 mm
Table size: Minimum 700 mm x 450 mm
Material: Steel frame with solid wheels with brakes
CE/GS approved
WARNING
Hazard of injury
Never stack the power modules on top of each other.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
CAUTION
Heavy load and potentially hot surface
Use protective gloves and safety shoes when handling the power modules.
Failure to follow these instructions can result in injury or equipment damage.
NOTE: Install the power modules starting from the bottom left slot. Install in the shown order, and start with the lowest number.

Front View

  1. Remove the filler plate from the empty power module slot. Save the filler plate for future use. Save the screws for reuse.

    Front View

  2. Use an appropriate scissor lifting cart to lift the power module to the correct height and push the power module into the power module slot.

    Front View

  3. Install the four screws in the left and right sides of the power module. Reuse the screws from step 1.

    Front View

  4. Set the enable switch on the power module to the ON (locked) position.

    Front View

DANGER
Hazard of electric shock, explosion, or arc flash
All power module slots must have either a power module or a filler plate installed.
Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?