990-55111E-001

Remove the Front Doors from the UPS

  1. Remove the packaging bag (marked (A) in the illustration) without cutting it – save the packaging bag (A) for later use.
  2. Open the front doors.
  3. Disconnect the display signal cable and the two LED strip signal cables from the cabinet. Roll up and fasten the signal cables to the doors so they do not get damaged.
  4. Remove kit 0M-18450 (bag with spring washers) from the documentation compartment in the right front door and save for later use.
  5. Remove the front doors. Store the front doors safely until reinstallation.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?