990-55111E-001

Final installation

  1. Reinstall the long narrow covers and the non-Class 2/non-SELV protection cover over the non-Class 2/non-SELV signal terminals.

    Front View

  2. Remove the plywood plate and the dust protection label from the top of the UPS.

    Front View

  3. Reinstall the front doors.
  4. Reconnect the display signal cable and the two LED strip signal cables to the cabinet.
  5. Close and lock the front doors.
  6. Remove the protective film from the UPS display in the front door.
  7. Cut the protective bag as indicated. Cover the UPS with the protective bag (marked (A) in the illustration) until commissioning to protect against dust and contaminants.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?