990-55111E-001

Mount the Seismic Anchoring and Position the UPS

Use the optional seismic anchoring kit GVXLOPT002 for this procedure.

DANGER
hazard of electric shock, explosion, or arc flash
Cover the UPS system with the packaging bag while making anchoring holes to prevent dust or other conductive particles from entering the system.
Failure to follow these instructions will result in death or serious injury.
WARNING
hazard of tilting
All rear and front seismic anchoring brackets must be installed.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
  1. Cover the UPS with the packaging bag (marked (A) in the illustration) to protect against dust from drilling in the floor. Roll up the rear side of the packaging bag, so the rear bottom part of the UPS (marked (B) in the illustration) is free.
  2. Place the rear seismic anchoring bracket for the UPS in the final installation area.
  3. Mark the 10 hole locations on the floor.

    Front View

  4. Drill the 10 anchoring holes according to national and local requirements.
  5. Mount the rear seismic anchoring bracket to the floor. Use appropriate hardware for the floor type – the hole diameter in the rear seismic anchoring bracket is ø16 mm. Minimum requirement is M12 strength grade 8.8 hardware (not provided).
  6. Use a bubble-leveler to ensure that the rear seismic anchoring bracket is level. Use the leveling shims if necessary.
  7. Push the UPS into position against the rear seismic anchoring bracket - the UPS will connect to the conic outcroppings on the rear seismic anchoring bracket.
    CAUTION
    Risk of equipment damage
    When pushing the UPS into position, push on the frame to avoid damaging the signal cables/plates.
    Failure to follow these instructions can result in injury or equipment damage.
  8. Fasten the cabinet to the rear seismic anchoring bracket by tightening the bolts. Torque to 50 Nm (36.87 lb-ft).

    Front View

  9. Lower the two front feet on the UPS until they have full contact with the floor – use a bubble-leveler to ensure that the cabinet is level.

    Front View

  10. Remove the eight M8x30 screws from the front of the UPS. These screws are needed for the front seismic anchoring bracket.

    Front View

  11. Install the front seismic anchoring bracket on the UPS with two M8x30 screws.

    Front View

  12. Mark the 10 hole locations on the floor.

    Front View

  13. Remove the front anchoring bracket from the UPS. Secure the packaging bag against the UPS with tape to create a seal.
    NOTE: The packaging bag must be tight against the frame to protect the power modules from dust when drilling holes in the floor.
  14. Drill the 10 anchoring holes according to national and local requirements.
  15. Remove the packaging bag from the UPS without cutting it – save the packaging bag for later use.
  16. Reinstall the front seismic anchoring bracket on the UPS with the eight reused M8x30 screws.

    Front View

  17. Mount the front seismic anchoring bracket to the floor. Use appropriate hardware for the floor type – the hole diameter in the front seismic anchoring bracket is ø16 mm. Minimum requirement is M12 strength grade 8.8 hardware (not provided).

    Front View

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?