Prepare the UPS for Top Cable Entry
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
- Prepare for power cables:
- Remove the gland plate for power cables from the top of the UPS.
- Drill/punch holes for power cables or conduits/grommets in the gland plate for power cables. Install conduits/grommets (not provided), if applicable.
- Reinstall the gland plate for power cables.
- Route the power cables into the UPS as shown.
- Remove the non-Class 2/non-SELV protection cover from the non-Class 2/non-SELV signal terminals. Remove the long narrow covers.
- Prepare for signal cables:
- Remove the gland plates and brush plates from the top of the UPS.
- For installation without conduits/grommets: Reinstall the brush plates.
- For installation with conduits/grommets: Drill holes in the gland plates for conduits/grommets, install conduits/grommets (not provided), and reinstall the gland plates.
- Route the signal cables into the UPS as shown to separate the Class 2/SELV cables from the non-Class 2/non-SELV cables.
DANGER