990-55111E-001

Position the UPS without Seismic Anchoring

  1. Push the UPS into position.
  2. Lower the front and rear leveling feet on the UPS with a wrench until they have full contact with the floor. The casters must not have contact with the floor. Use a bubble-leveler to check that the UPS is level.
    NOTICE
    Risk of equipment damage
    Do not move the cabinet after the leveling feet have been lowered.
    Failure to follow these instructions can result in equipment damage.

    Front View

    NOTE: For installations with limited rear access, only lower the two front feet.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?