990-55333C-018

適合規格

安全管理 IEC 62040-1: 2017, Edition 2.0, Uninterruptible Power Systems (UPS) - Part 1: Safety requirements
EMC/EMI/RFI IEC 62040-2: 2016, 3rd edition Uninterruptible Power Systems (UPS) - Part 2: Electromagnetic compatibility (EMC) requirements C3
IEC 62040-2: 2005, 2nd edition Uninterruptible Power Systems (UPS) - Part 2: Electromagnetic compatibility (EMC) requirements C3
性能 性能基準:IEC 62040-3: 2021-04, 3rd edition Uninterruptible Power Systems (UPS) - Part 3: Method of specifying the performance and test requirements.IEC 62040-3の5.3.4項に準拠した出力性能分類:VFI SS 11
輸送 IEC 60721-4-2 Level 2M2
接地システム TN、TNC、TN-S、TNC-S,TT*
過電圧カテゴリ OVC III
保護クラス I
汚染度 2
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

この情報は役に立ちましたか?