GEX7904402-00

Main characteristics

  • Easy to install: The device can be mounted on a panel using two retainer clips. This is a compact meter with 49 mm meter depth behind the panel that can connect up to 480 V + 10% AC L-L without voltage transformers for installation compliant with measurement category III, and double insulated.

  • Easy to operate: The device has intuitive navigation with self-guided menus and heartbeat LED that indicate normal functioning of your device. It also conveys the communication status when connected to an RS-485 network.

  • LED display: The device has intuitive navigation with self-guided four buttons, 8 segment alpha-numeric LED, and three lines of concurrent values with Kilo and Mega value indicator.

  • Standard compliance:

    • Accuracy Class 1.0 for V AF PF metering

    • CE certification as per IEC 61010-1 Edition 3.1

    • cULus as per UL61010-1 and CAN/CSA-C22.2 IEC 61010-1 Edition 3.1, for 480 V AC L-L

    • EMI / EMC tests as per IEC 61326-1

  • CT nominal: 5 A or 1 A nominal current (field settable).

  • Password: Field configurable password to secure set up information and prevent tampering of integrated values.

  • Display: The device has an auto scale and auto range display capability that provides 4 digits for Instantaneous parameters.

  • Analog load bar: The device’s front panel has a colour-coded analogue load bar that indicates the percentage of load through 12 LED with the option to select full scale based on connected load.

  • Suppression current: The meter can be configured to disregard the measurement of induced / auxiliary load current in the circuit (can be set from 5 to 99 mA).

  • Time counters: For measuring meter ON hours and power interruptions

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?