GEX7904402-00

Panel meter

LED indicators

The LED indicators alert or inform you of meter activity or status. Refer to the image below for the various LED indicators the meter provides.

A

Heartbeat / serial communications LED (Green)

Energy pulse output LED (Red)

Rear wiring

The meter provides current and voltage inputs along with other wiring options. Refer to the image below for various wiring options the meter provides.

A Input voltage terminals (V1, V2, V3, VN)
B Auxiliary power supply (control power) terminals (L1, L2)
C RS-485 communications terminals ( METSEGLDM3141 only) (D1+, D0-)
D Input current terminals (I1+, I1- , I2+ , I2- , I3+ , I3-)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?