GEX7904402-00

Applications

The meters can be used in various cost management and network management application. Some of the import applications are mentioned below.

Cost management

  • Electrical installation remote monitoring

  • Motor control centres

  • Control panels

  • Power distribution boards

  • Original equipment manufacturers (OEMs)

  • Building management system

  • Panel instrumentation

  • Energy management system

Network management

  • Measurement of power factor

  • % unbalance for voltage and current

  • Phase angle between the respective voltage and current phase

  • Modbus RTU protocol, RS-485 communication port for integration with energy management systems ( METSEGLDM3141 only)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?