GEX7904402-00

Power factor sign convention

Power factor sign (PF sign) can be positive or negative, and is defined by the conventions used by IEC standards.

PF sign convention: IEC

PF sign correlates with the direction of real power (kW) flow.

  • Quadrant 1 and 4: Positive real power (+kW), the PF sign is positive (+).

  • Quadrant 2 and 3: Negative real power (-kW), the PF sign is negative (-).

IEC -1 to +1 format

Quadrant

PF Range

HMI Representation with sign

PF in RS-485 Comm

(Reg IEC format)

Quadrant 1

0 to +1

Inductive (+)

Positive Sign

Quadrant 2

-1 to 0

Capacitive (-)

Negative sign

Quadrant 3

0 to -1

Inductive (-)

Negative Sign

Quadrant 4

+1 to 0

Capacitive(+)

Positive Sign

Sample screen

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?