GEX7904402-00

RMS page

To view RMS parameters:

  1. From the Home (RMS) page, use Up or Down button to navigate to RMS.
  2. Press OK.
  3. Press the Up or Down button to navigate to the next RMS parameter.
  4. Press Left button to exit.

Parameter navigation

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?