GEX7904402-00

Meter types

The GLDM3141 series is available in one physical form factor.
Commercial reference Description

METSEGLDM3141

Class 1 panel mount meter with RS-485 and integrated display.

METSEGLDM3141NC

Class 1 panel mount meter with integrated display.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?