GEX7904402-00

Button functions in viewing parameters

Mode Button Description Function
Display mode
NOTE: Display mode is view-only and displays the parameter values.
Down key: To navigate down To view the next parameter value.
Up key: To navigate up To view the previous parameter value.
Right / OK key: To navigate right / Enter key To move from one page to the next.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?