GEX7904402-00

Setup screen menus

Setup screen enables you to configure various setup parameters.

The meter’s display screen and buttons allow you to navigate to and edit the required parameters.

To enter into setup:

  1. From the Home page, use Up or Down button to navigate to Maintain.
  2. Press OK.
  3. Use Up or Down button to navigate to Set.
  4. Press OK.
  5. Enter the password. Default password is 0000.
  6. Press OK to enter Setup.
  7. Press Left button to exit Setup after viewing parameters.

Below is the list of setup parameters and the configurations it supports.

Setup menus:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?