GEX7904402-00

Meter overview

The GLDM3141 series meters offer comprehensive 3-phase electrical instrumentation and load management facilities in a compact and rugged package.

The GLDM3141 meters offer value for the demanding needs of your energy monitoring and cost management applications. Meters in the series range comply with Class 1.0 accuracy standards and feature high quality, reliability and affordability in a compact and easy to install format.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?