Analog load bar
-
Unique indication of total load % with respect to the full scale through the 12 LED at the right side of the display.
-
A bar graph indicating 10% load through each LED.
-
The load bar help in finding the total load. To calculate total load, count the number of illuminated LED, and multiply by 10.
Load percentage and bar graph indication
| Load percentage | Bar graph display |
|---|---|
| Less than 10% | No LED is lit. |
| Between 10% to 40% | Amber LED get lit. |
| Between 50% to 80% | Green LED get lit to indicate that the load is acceptable and should not be increased further. |
| Above 80% | Red LED get lit to indicate that the load has exceeded the sanctioned limit and is dangerous. |
Indicators
Kilo, Mega, and negative
Decimal point scaling
Giga (M+K), Mega (M), Kilo (K), and decimal point scaling - RMS, Current and Voltage
| RMS Reading | Indicator |
|---|---|
| Less than 0.001 | K, M OFF, displays 0.000 |
| Less than 9999 | K, M OFF |
| Above 9999 | K ON, M OFF |
| Above 9999 K | M ON, K OFF |
| Above 9999 M | Giga (K + M indicators ON) |
| Up to 9999 G | Giga |
| Above 9999 G | Display shows Hi |
RMS readings are four digits. The maximum number the meter handles is 9,999 G for RMS.