DOCA0239EN-09

Version 2.4.1

New Features

Implemented Power Interface with IO avatar in IO Optimization.

Known Issues

  • When Avatar modification is done after Device Optimization, then user needs to recheck in to the IO PORT ASSIGNMENT for that avatar.

  • DTM will automatically changes product code in configuration based on discovered topology.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?