DOCA0239EN-09

Version 2.4.3

New Features

  • Configurable Fallback Mode

    For starters and IO module outputs, the fallback position can be configured for each Avatar except Power Interface Avatar.

  • Additional Avatar trip status are available in the IO PORT ASSIGNMENT table

  • Configurable communication loss timeout for Fieldbus Protocol

Bugs Fixed

DTM will automatically changes product code in configuration based on discovered topology.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?