DOCA0239EN-09

Version 2.4.0

NOTE: If firmware upgrade is to be done from 001.100.013/002.100.016 to 003.000.001, then it has to be performed two times.
  1. Perform an upgrade from 001.100.013/002.100.016 to 002.200.008/002.300.006.

  2. Perform an upgrade from 002.200.008/002.300.006 to 003.000.001.

NOTE: Function blocks library for PLCs with Machine Expert on Modbus TCP protocol is not compatible.

Workaround: Use the Schneider Electric Machine Expert Modbus TCP PLCs as a third party PLC.

New Features

  • IO Optimization

    IO Optimization feature allows users to share their I/O devices between different avatars and optimize them to reduce the number of I/O devices required per TeSys island.

    User may also utilize Device Optimization feature which will permanently remove free AIOM/DIOM devices from the TeSys island configuration.

  • Rearrange Avatar(s)

    Introduces the functionality to automatically try and resolve the warnings like electromagnetic interference and mounting positions by changing the position of avatar(s) in question.

  • Local Control

    Local control functionality is extended to the safe category avatars.

  • Local Trip Reset

    Introduces the functionality to reset the trips locally at individual avatar level. Resetting trips at TeSys island level through remote is still available through the control panel as before.

  • Vertical Orientation

    Introduces a new information message about derating to be applied when mounting position is selected as vertical.

Bugs Fixed

  • Load from device does not work when there are more than 16 SIL starters in the configuration.

  • After reconnecting to the device, the forced mode status indication of avatar input is not correct for Motor Two Speeds avatar.

Known Issues

The following are the known issues in this version for TeSys island DTM Library:

  • TeSys island DTM Library does not work with EcoStruxure Control Expert V15.2.

    The issue is because DHCP is enabled without a role name associated.

    Workaround: Open the M580 DTM and add the role name in the address setting of theTeSys island instance.

  • Creation of I/O Avatars as part of IO Optimization and deletion of I/O modules as part of Device Optimization does not work, when the users reopens saved project without visiting MY AVATAR tab.

    Workaround: Open the saved project and visit MY AVATAR tab before clicking IO Optimization and Device Optimization.

  • Power Interface with IO avatar can not be used in IO Optimization.

  • This release is not applicable for SIL starters.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?