DOCA0239EN-09

Version 2.2.2

New Features

The following new features are added in this version for TeSys island DTM Library:

  • EcoStruxure Control Expert Classic v15.0 SP1 and later

  • PLC Modicon M580 series

Known Issues

The following are the known issues in this version for TeSys island DTM Library:

  • EcoStruxure Control Expert Classic support

    • Only DTM version 2.2.2 or later works with EcoStruxure Control Expert Classic software

    • Supports only PLC Modicon M580 (Modicon M340 not supported)

    • Supports only Modbus TCP protocol (Ethernet or IP support not supported)

      NOTE: To add the TeSys island DTM Library in the EcoStruxure Control Expert Classic software, select Modbus over TCP protocol in Add window. For more information, refer to the EcoStruxure Control Expert Classic - Quick Start Guide.

  • It is recommended to choose short and meaningful names for DTM instances in DTM browser of EcoStruxure Control Expert.

  • For Analog IO Avatar, Analog output type value 4 mA or 20 mA does not work. It is recommended to use the value 0 mA or 20 mA.

  • When the TeSys island DTM instance is copied and pasted in the Control Expert DTM browser, the DDT types for new TeSys island is not displayed unless the solution is built.

  • In Diagnostics > Counters > Trip Record Register table for switch avatar, the trip timestamp is not displayed as expected.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?