DOCA0239EN-09

Version 2.4.2

NOTE: Korean language can be used only with SoMove V2.9.5 or later.

New Features

User interfaces for TeSys island DTM are supported in Korean language.

KC (Korean Certification) will be applicable to the below commercial references:

In scope

TPRBCEIP

Ethernet/IP bus coupler

TPRBCPFN

PROFINET bus coupler

TPRDG4X2

Digital I/O module

TPRST009

9 A standard starter

TPRST025

25 A standard starter

TPRST038

38 A standard starter

TPRST065

65 A standard starter

TPRST080

80 A standard starter

TPRVM001

Voltage interface module

TPRAN2X1

Analog I/O module

Out of scope

TPRBCPFB

PROFIBUS bus coupler

TPRPM009

9 A Power inteface module

TPRPM038

38 A Power inteface module

TPRPM080

80 A Power inteface module

TPRSM001

SIL interface module

TPRSS009

9 A SIL starter

TPRSS025

25 A SIL starter

TPRSS038

38 A SIL starter

TPRSS065

65 A SIL starter

TPRSS080

80 A SIL starter

Bugs Fixed

Creation of I/O Avatars as part of IO Optimization and deletion of I/O modules as part of Device Optimization does not work, when the user reopens saved project without visiting MY AVATAR tab.

Known Issues

Korean language is not supported by SoMove software.The TeSys island DTM text will be viewed in Korean by choosing the Korean language option in SoMove software. The text which comes from SoMove software is displayed in English.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?