DOCA0239EN-09

DTM Overview

The DTM (Device Type Manager) is used together with FDT container (Field Device Tool container, also referred to as FDT frame) to commission and diagnose TeSys island. The combination of FDT and DTM is also called commissioning software.

Once a DTM is installed, it can be used by different FDT containers.

Examples of FDT containers:

  • SoMove software (Schneider Electric)

  • fdtCONTAINER (M&M Software GmbH)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?