DOCA0239EN-09

Version 3.0.0

@Updated D1

New Features

IO Optimization feature extension to EcoStruxure Control Expert and EcoStruxure Automation Expert-Motion function blocks library.

Bugs Fixed

Alarms and trips information is not proper in exported L5X files (Acyclic.L5X and AOI.L5X) from DTM.

Known Issues

Voltage Fluctuation Status Reset is not functioning in DIAGNOSTICS power voltage section.

Workaround: User can Reset Voltage Fluctuation Status from ENERGY MONITORING power voltage section.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?