DOCA0239EN-09

Version 2.3.0

New Features

Dahlander motor control is added for Motor Two Speeds avatar.

Known Issues

The following are the known issues in this version for TeSys island DTM Library:

  • Load from Device does not work when there are more than 16 SIL starters in the configuration.

    This issue exists in all the previous TeSys island DTM Library versions.

    Workaround: Save the configurations in SoMove or EcoStruxure Machine Expert software and connect to the device without using Load from Device.

  • After reconnecting to the device, the forced mode status indication of avatar input is not correct for Motor Two Speeds avatar.

    Workaround: Close and open the project again in the configuration software.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?