DOCA0239EN-09

Operating Systems

The following operating systems are supported for TeSys island DTM Library:

  • Microsoft Windows 7 SP1 32 or 64-bit

  • Microsoft Windows 10

NOTE: For Windows 7 SP1 machines, install the package from the Microsoft Download Center to enable support of TLS 1.22 before installing the TeSys island DTM Library.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?