DOCA0272EN-00

Installing SoMove™ Software and TeSys™ island DTM

To generate the AML configuration files for import into the Siemens® TIA Portal, you must install SoMove™ software and the TeSys™ island Device Type Manager (DTM). These tools provide the necessary features to configure the TeSys™ island and download the configuration to the bus coupler.

To download the SoMove software, go to https://www.se.com/us/en/product-range-download/2714-somove/#/software-firmware-tab.

To download the TeSys island DTM library, go to https://www.se.com/us/en/product-range-download/65746-tesys-island/#/software-firmware-tab.

For detailed instructions on the installation and usage of these tools, refer to the TeSys™ island DTM Online Help Guide, document number 8536IB1907.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.