DOCA0272EN-00

Supported Members of UDT_Control

Not all members of the user defined type “UDT_Control” (see UDT_Control) are supported by all avatars. The following table gives an overview of which elements are available for this avatar. Unsupported values will always use the default value.

NOTE: Safety Integrity Level according to standard IEC 61508.

Elements

Element

Sub-Element

Supported

MotorTemperature

n/A

No

SILGroup

n/A

Yes

ThermalCapacity

n/A

No

AlarmMsg1

GroundCurrent

Yes

ThermalOverload

No

PhaseUnbalance

Yes

UnderCurrent

No

AlarmMsg2

OverCurrent

No

MotorOverheat

No

TripMsg1

GroundCurrent

Yes

ThermalOverload

No

LongStart

No

Jam

No

PhaseUnbalance

Yes

UnderCurrent

No

Stall

No

TripMsg2

PhConfig

Yes

OverCurrent

No

PhaseLoss

Yes

PhaseReversal

Yes

MotorOverheat

No

TimeToTrip

n/A

No

TimeToReset

n/A

No

PAStatusReg1

PA0Status

No

PA1Status

No

PA2Status

No

PA3Status

No

PA4Status

No

PA5Status

No

PA6Status

No

PA7Status

No

PA8Status

No

PA9Status

No

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?