DOCA0272EN-00

Supported Members of UDT_Control

Not all members of the user defined type “UDT_Control” (see UDT_Control) are supported by all avatars. The following table gives an overview of which elements are available for this avatar. Unsupported values will always use the default value.

NOTE: Safety Integrity Level according to standard IEC 61508.

Elements

Element

Sub-Element

Supported

MotorTemperature

n/A

Yes

SILGroup

n/A

No

ThermalCapacity

n/A

Yes

AlarmMsg1

GroundCurrent

Yes

ThermalOverload

Yes

PhaseUnbalance

Yes

UnderCurrent

Yes

AlarmMsg2

OverCurrent

Yes

MotorOverheat

Yes

TripMsg1

GroundCurrent

Yes

ThermalOverload

Yes

LongStart

Yes

Jam

Yes

PhaseUnbalance

Yes

UnderCurrent

Yes

Stall

Yes

TripMsg2

PhConfig

Yes

OverCurrent

Yes

PhaseLoss

Yes

PhaseReversal

Yes

MotorOverheat

Yes

TimeToTrip

n/A

Yes

TimeToReset

n/A

Yes

PAStatusReg1

PA0Status

No

PA1Status

No

PA2Status

No

PA3Status

No

PA4Status

No

PA5Status

No

PA6Status

No

PA7Status

No

PA8Status

No

PA9Status

No

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?