Supported Members of UDT_Control
Not all members of the user defined type “UDT_Control” (see UDT_Control) are supported by all avatars. The following table gives an overview of which elements are available for this avatar. Unsupported values will always use the default value.
Elements
|
Element |
Sub-Element |
Supported |
|---|---|---|
|
MotorTemperature |
n/A |
No |
|
SILGroup |
n/A |
Yes |
|
ThermalCapacity |
n/A |
No |
|
AlarmMsg1 |
GroundCurrent |
Yes |
|
ThermalOverload |
No |
|
|
PhaseUnbalance |
Yes |
|
|
UnderCurrent |
No |
|
|
AlarmMsg2 |
OverCurrent |
No |
|
MotorOverheat |
No |
|
|
TripMsg1 |
GroundCurrent |
Yes |
|
ThermalOverload |
No |
|
|
LongStart |
No |
|
|
Jam |
No |
|
|
PhaseUnbalance |
Yes |
|
|
UnderCurrent |
No |
|
|
Stall |
No |
|
|
TripMsg2 |
PhConfig |
Yes |
|
OverCurrent |
No |
|
|
PhaseLoss |
Yes |
|
|
PhaseReversal |
Yes |
|
|
MotorOverheat |
No |
|
|
TimeToTrip |
n/A |
No |
|
TimeToReset |
n/A |
No |
|
PAStatusReg1 |
PA0Status |
No |
|
PA1Status |
No |
|
|
PA2Status |
No |
|
|
PA3Status |
No |
|
|
PA4Status |
No |
|
|
PA5Status |
No |
|
|
PA6Status |
No |
|
|
PA7Status |
No |
|
|
PA8Status |
No |
|
|
PA9Status |
No |