PN_Control_Motor_One_Direction_SS_C1/2 (PROFINET IO)
The following tables give information about the parameters of the function block interface.
Inputs
|
Input |
Data Type |
Description |
Variable Category |
|---|---|---|---|
|
i_xEnable |
BOOL |
Activates the function block processing. Cyclic data will be read/written to the hardware IO interface. |
Function block control |
|
i_xRunFwd |
BOOL |
If this input is TRUE, the avatar forward switch is closed. |
Cyclic data |
|
i_xTripReset |
BOOL |
If this input is set to TRUE, detected trips whose trip reset conditions have been met will reset for this avatar. |
Cyclic data |
|
i_xAcyclicBusy |
BOOL |
Can be used to block the acyclic execution if acyclic communication of another function block is active. |
Function block control |
|
i_xExecute |
BOOL |
Starts an acyclic request on a rising edge. |
Function block control |
|
i_hwSubmHWID |
HW_IO |
Must correspond to the hardware identifier of the acyclic submodule of the related avatar to be able to execute the acyclic communication. |
Communication parameter |
|
i_hwStartAddress |
Variant |
Must correspond to the first address of the cyclic input submodule address range of the related avatar to be able to execute cyclic read communication. |
Communication parameter |
In/Out
|
InOut |
Data Type |
Description |
Variable Category |
|---|---|---|---|
|
iq_hwQWAddress |
WORD |
Must correspond to the address of the cyclic output submodule to be able to execute cyclic write communication. |
Communication parameter |
Outputs
|
Output |
Data Type |
Description |
Variable Category |
|---|---|---|---|
|
q_xActive |
BOOL |
If this output is set to TRUE, the Avatar function block is enabled, or an acyclic request is busy. |
Function block status |
|
q_xError |
BOOL |
If this output is set to TRUE, a detected error occurred while executing the Avatar function block. For detailed information about the detected error, see the value of the Error ID. |
Function block status |
|
q_dwErrorID |
DWORD |
The Error ID shows detailed information about the detected error that occurred. Possible values are shown in the table below. |
Function block status |
|
q_dwAcyclicStatus |
DWORD |
The Acyclic status provides detailed information about the acyclic fieldbus communication, including detected error details. For detailed information about the status values, see Function Block Library. |
Function block status |
|
q_xAcyclicBusy |
BOOL |
If this output is set to TRUE, an acyclic request is still busy. |
Function block status |
|
q_xReady |
BOOL |
Indicates TRUE if the function block is ready to receive an Execute command. |
Cyclic data |
|
q_xUpstrVPres1 |
BOOL |
If this output is set to TRUE, the avatar has detected that upstream main power is present for the first starter/power device in this avatar. |
Cyclic data |
|
q_xRunFwd |
BOOL |
If this output is set to TRUE, the avatar forward switch is closed. |
Cyclic data |
|
q_xLoadStart |
BOOL |
If this output is set to TRUE, the motor is in start phase. |
Cyclic data |
|
q_xLoadRun |
BOOL |
If this output is set to TRUE, a Run or Close command has been executed, and current is flowing in the poles (equivalent to motor running but also for non-motor avatars). |
Cyclic data |
|
q_xAlarm |
BOOL |
If this output is set to TRUE, a protection alarm has been detected by the avatar. |
Cyclic data |
|
q_xTripped |
BOOL |
If this output is set to TRUE, a protection trip event has been detected by the avatar. |
Cyclic data |
|
q_xReadyToReset |
BOOL |
If this output is set to TRUE, the avatar meets the trip reset conditions and can be reset with a Trip Reset command. |
Cyclic data |
|
q_xAssetAlarm |
BOOL |
If this output is set to TRUE, a power device or SIL* Starter within the avatar has reached or exceeded 90% of the expected durability (per the avatar parameter). |
Cyclic data |
|
q_udiIRMSAvg |
UDINT |
Indicates the average of the most recent phase current Irms values. (Unit: A) |
Cyclic data |
|
q_udtControl |
UDT_Control |
This is a structure of acyclic status data for Control avatars, which includes information about alarm and trip messages and maintenance information about the avatar. For detailed information about the structure of this UDT, see UDT_Control. For an overview of which members of the UDT are supported by this avatar, see Supported Members of UDT_Control. |
Acyclic data |
Status and error codes from ConstTeSysIsland
|
Member name |
Used by the function block |
|---|---|
|
Cdw_ErrNoMsg |
Yes |
|
Cdw_ErrInternal |
Yes |
|
Cdw_ErrInvalidCycInAddr |
Yes |
|
Cdw_ErrInvalidHwid |
Yes |
|
Cdw_ErrInvalidNumOfAvatars |
No |
|
Cdw_ErrReadCycIn |
Yes |
|
Cdw_ErrReadAcycData1 |
Yes |
|
Cdw_ErrReadAcycData2 |
No |
|
Cdw_ErrWriteAcycData |
No |
|
Cdw_StsReadAcycData1Compl |
Yes |
|
Cdw_StsReadAcycData2Compl |
No |
|
Cdw_StsWriteAcycDataCompl |
No |