DOCA0272EN-00

Installation requirements

To make full use of the function block library for the TIA Portal described here, we recommend you use it in the context of the full TIA Portal integration for TeSys island. Beyond installing the function block library, this usage requires installation of the device descriptions for TeSys island for PROFIBUS DP, PROFINET IO, or both. In addition, the AML import/export functionality for island configuration requires installation of the optional TIA Portal package, “TIA Portal Openness”.

For more information about the usage and installation of the other parts of the TeSys island TIA Portal integration, as well as instructions on how to import the function block library into the TIA Portal, refer section Import a Library Function Block into a TIA Portal Project.

NOTE: We recommended that you read the sections Software Installation and Integration Procedure, before using the TeSys island function block library for the TIA Portal.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?